AXIS#.FIELDWEAKENING.VOLTFILTERBW
Description
This keyword determines the bandwidth of the second order low-pass biquad filters that are applied on the q-axis and d-axis voltages for noise reduction. These voltages are used inside the field weakening algorithm for regulating the motor-voltage-vector-magnitude when operating above base speed. Lower bandwidths result in cleaner signals but can also create phase lag and lower the phase margin of the system. Depending on the required speed of the motion, they can be adjusted.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-06-00-000 |
|
General Information
|
Type |
Read/Write |
|
Units |
Hz |
|
Range |
0 to 5000 Hz |
|
Default Value |
1500 Hz |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
Yes |
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.FIELDWEAKENING.VOLTFILTERBW |
5019h |
04h |
Signed32 |
- |
- |
Read/Write |
No |
|
AXIS2.FIELDWEAKENING.VOLTFILTERBW |
5119h |
04h |
Signed32 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
7302 |
1 |
7302 (0x1c86) |
AXIS1.FIELDWEAKENING.VOLTFILTERBW |
Signed32 |
Read/Write |
Yes |
|
72838 |
2 |
7302 (0x1c86) |
AXIS2.FIELDWEAKENING.VOLTFILTERBW |
Signed32 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.FIELDWEAKENING.VOLTFILTERBW |
7302 |
Signed32 |
Read/Write |
- |